Other Parts Discussed in Thread: LMK04228, LMK5C33216
Hello,
I have an application where I use a 10 MHz reference which will lock a 100 MHz VCXO through a digital PLL.
The equipment will work with an external reference and additionally, it has an internal 10 MHz reference which will be used as back-up solution when the external reference is not available.
I would need a solution which could act over the control voltage of the internal OCXO reference, so if the external reference fails the ouutput frequency of the 100 MHz VCXO continues being exactly the same when it will lock to the internal reference. If the equipment is switched on without external reference, the output frequency when operating with internal reference must be exactly th frequency configured in factory.
Could you recommend me a circuit to implement this functionality?
Thanks in advance for your support and advices.