Other Parts Discussed in Thread: LMK1D1204P
I am evaluating the LMK1D1204P and LMK1D1208I, and comparing the current consumption vs frequency graphs. It appears that these graphs in the data sheets are exactly the same for both of these devices, even down the figure numbering (figure 6-1).
Given that the devices are 8 output, and 4 output devices respectively I am worried there is a problem in one of the data sheets and would like to confirm the current consumption for both devices is supposed to be approximately the same.
Additionally, I want to ensure that the current consumption graphed for each devices is the current for a given frequency with all outputs enabled for both devices. If the answer is not can you provide information so that I may calculate the power draw for my given situation.
Thanks