Part Number: LMX2592
We've been using the LMX2592 Synthesizer for several years. Looking at the RF power output in detail, we see shifts in the output at ~1200MHz to 1700MHZ & 3400MHZ. We assume this is due to different internal VCOs being used. I have a spreadsheeet showing this if it would be hopeful to you to understand what we're seeing. Issue is, we've try to set the power output levels dynamically to create a flat output power, but it doesn't look possible due to the radical power ranges at different frequencies.
Is the behavior normal?