Hi Team:
When I configure the LMX2820 encountered the following problems:
1,Fosc=100M,the output is 200M;the den=1,000,000,and resolution is 100Hz;
2,when the output=200M+100Hz,the configure as follow:
it can lock!and the output is right!
3,when the output=200Mhz-100Hz:
It can‘t output,read the reg74,rb_LD=0x2,but the LD pin is low level;
4,Does it have anything to the fraction NUM and INST_CAL_PLL_NUM value?
Are there any other registers need to adjust?
5,In application, set it up via the MCU SPI.
Look forward to your help! Tks!