Part Number: LMX2433EVAL
Other Parts Discussed in Thread: LMX2433, LMX2430, USB2ANY, LMX2581, CODELOADER, USB2ANY-UWIRE
I can´t communicate the computer with the PLL.
I am using a HPA665-001 to program LMX2433EVAL board. Between both is SV600857-001 (USBANY-UWIRE). This board has a lot of jumpers. In the user´s guide of LMX2430/33/34 Evaluation board, page 23, there is a table with different configurations to different devices, but not to LMX2433.
The question is: which is the right jumpers configuration??.
The HPA665 is right connected to the lap, I can see a serial number, I suppose, if I push on identify button, also I see the USB2ANY port setup.
On the other hand if I push the load device button (in keyboard controls) the system does not send any error message.
Thanks