This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2694-SEP: Differential termination for unused RFOUTB

Part Number: LMX2694-SEP

We will not be using RFOUTB and will configure R44 to power down this output.  Figure 8-7 (Termination of Unused Output - Differential) in the datasheet shows to use 11 parts to terminate an unused output... 11 parts!  Is this correct?  4 of these parts are for biasing the unused buffer amplifier which will be powered down.  Is this really the correct method of terminating and unused differential output, or can it simply be open-circuited or have a 100 ohm resistor across the differential pins?  We are using 3 of these in our design and PCB real estate is limited, so it would be nice to reduce parts where possible.  Thanks, Chris