Part Number: BQ32000
In External RTC BQ32000 facing issues.
while reading the minutes register(0x01) we found that the oscillator failure flag(OF) is set.But the time was incremented properly.
As per the data sheet if flag is set it can be cleared through serial interface.
But As we observed that the occurence of the failure flag is random
So, We need to know the probable outcome of the below mentioned instances
1. Since the time is updating properly, what will happen if we didn't clear oscillator failure flag(OF) register.
2. Is clearing the flag is mandatory?
3. What if the failure Flag occurrence is very frequent