Dear Team,
Is there any way (programing) to adjust the output slew rate and rise/falling time?
We have failure slew rate at Y2 and rising/falling time at Y3.

Failure slew rate at Y2


Failure rising/falling time at Y3


Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Is there any way (programing) to adjust the output slew rate and rise/falling time?
We have failure slew rate at Y2 and rising/falling time at Y3.

Failure slew rate at Y2


Failure rising/falling time at Y3


Many Thanks,
Jimmy
Jimmy,
First, I should note - the slew rate and the rise/fall time go hand in hand. If the slew rate is decreased, and the voltage differential is the same, then the rise time must increase - they are inversely proportional.
We specify a typical slew rate for LVDS, but not a minimum or maximum - what may be better is to consider setting the CDCI6214 for a different output format and using external components as needed.
See the below image as an example for converting an LVPECL driver output to an LVDS signal for a receiver:

The only difference here is that the 150-Ohm resistors would not be used on the LVPECL driver side.
The LVPECL swing meets the criteria, with the typical rise time reduced from 657 ps to 500 ps - this should be enough of a reduction to meet the standards.
Thanks,
Kadeem