Part Number: LMX2595
We are using the this part at -40C in Full Assist mode and see evidence that the Vtune voltage is railing to ground (have not probed on it yet, it is not real easy for us to do at cold). We plan on confirming the voltage next week. We expected to frequency to under or overshoot during frequency settling but for some transitions, it undershoots by about 12 MHz and stays there for 4-6 usec which causes a failure for us.
Here are the settings we are using during calibration:
PFD and state machine frequency: 200 MHz
ACAL_CMP_DLY20
PFD_DLY_SEL=1
We only have a problem at -40C, even -30C looks good. Should any of these settings be changed?