Part Number: CDCLVC1102
HI,
Attached my design for review,
I need to give 24MHZ clock to RSCLK pin of DSP and BITCLK of CODEC, Will this design work as is?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCLVC1102
HI,
Attached my design for review,
I need to give 24MHZ clock to RSCLK pin of DSP and BITCLK of CODEC, Will this design work as is?

Hi Amrutha,
Capacitive loading and series resistance can be reduce to get a proper swing. Even though the cutoff frequency is higher than your clock input. I would not use that excessive capacitive loading because rise and fall time of the signal is fast and it would result in filtering the sharp edges. You can try a 5 pF load cap value. Furthermore, the output impedance of the driver is around 45 ohm at 3.3 V. You can just add 5 ohm in series to match the transmission line impedance.
Let me know if this answers your question.
Best,
Asim