Part Number: LMK04828
Hi,
On page 45 of the data sheet revised on may 2020, it says there can be 2 ways to activate Duty cycle correction (DCC), which are:
1) Setting DCLKoutX_MUX=1
2) Setting DCLKoutX_MUX=3 and DCLKoutX_ADLY_MUX =1
However, in the example given on the bottom of the same page it says "DCLKoutX_MUX is set to be 1 and therefore DCLKoutX_MUX_ADJUST=0 since DCC is not enabled." Isn't it contradicting with above argument? if DCLKoutX_MUX=1 DCC is enabled thus DCLKoutX_MUX_ADJUST should be 1.