Part Number: TPL5111
Other Parts Discussed in Thread: TPL5110, TPL5010
I have been looking for an IC like the TPL5111 (but opposite sort of) which acts like a timed watchdog to hard reset a MCU. Under normal operation the MCU will 'report in' by pulsing an input pin on the watchdog which resets the timer. If the MCU is stuck in an unknown state and does not 'report in' the watchdog timer will timeout and pull the MCU's reset pin low to reset the MCU. Best thing I can think of is a 555 timer with an AND gate on the output of the 555 timer. The trigger (MCU reporting it is fine) also resets the 555 timer and an AND gate with the inputs of trigger and 555's output rectifies the 555's starting condition of 0V. I know I have solved my own problem but is there anything that would serve this purpose which integrates both and consumes less power?