This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In regards to my book, a more recent version is available at deanbanerjeepll.com and it is order from print from LULU press.
Most likely, the reason for the difference is that it is likely not exactly the same design. If the filter has k components, it needs k constraints.
This is why just giving phase margin and loop bandwidth is not enough to uniquely specify the components. PLLatinum Sim uses:
2nd order filter:
Loop Bandwidth, Phase Margin, Gamma
3rd Order Filter
Loop Bandwidth, Phase Margin, Gamma, T3/T1 pole ratio, Constraint that C3 is maximized
4th order filter:
Loop Bandwidth, Phase Margin, Gamma, T3/T1 Pole Ratio, T4/T3 pole ratio, Constraint that C4 is maximized
Note that for the case of the 4th order filter, there are 6 constraints, but 7 components, so actually it is possible to have more than one solution
But for 2nd & third order, it is unique.
The "Minimize Jitter" and other settings impact loop bandwidth, phase margin, Gamma, T3/T1 ratio, T4/T3 ratio, but do not directly impact the loop filter.
Regards,
Dean