Part Number: LMK61E2
Hello team,
Datasheet for LMK61E2 only provide the phase noise of 156.25MHz and 161.1328125MHz.
Can you provide 320MHz output phase noise data also?

Best Regards,
Austin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Austin,
Here is some phase noise data I took on the bench using the 320 MHz LVDS config generated by TICS Pro:
|
Offset |
Phase Noise (dBc/Hz) |
|
10 kHz |
-137.90 |
|
50 kHz |
-136.51 |
|
100 kHz |
-136.31 |
|
300 kHz |
-137.35 |
|
500 kHz |
-138.86 |
|
1 MHz |
-142.74 |
|
3 MHz |
-150.75 |
|
5 MHz |
-154.14 |
|
10 MHz |
-157.16 |
| 20 MHz | -159.02 |
Regards,
Connor