Other Parts Discussed in Thread: LMX2694-EP
Hi Team,
My customer Samsung is asking for a RF PLL solution in RRU.
I want to confirm whether there are any devices available at a non-space level that can support an ambient temperature (TA) greater than 85 degrees and an output frequency greater than 3600 MHz? Samsung's board temperature currently reaches 95 or 105 degrees. Do we have a solution that can support these conditions?
If not, do we have a chip that can output 3600 MHz under a board temperature of 95/105 degrees?
BR
Adrian