Part Number: LMK05028
Other Parts Discussed in Thread: LMK5B33216, LMK5C33216
Hi team,
My team is current using LMK05028 with INx frequency 388.8MHz, which is smaller than the maximum INx frequency rating.
However, it appears that due to the customer's FPGA issue, sometimes FPGA output frequency goes to 777.6MHz, which is 2 times higher than their current frequency, and exceeded the max INx frequency rating.
The maximum INx rating on the datasheet is 750MHz, using 777.6MHz surpass the maximum rating by 27.6MHz. Is this over frequency also supported as a part of the margin, or will it cause any issue or malfunction to the device?
Regards