Hello,
I would need to be able to synchronize a clock on 32 PCB modules. By this I mean making sure that the clocks of each module can be triggered simultaneously with a starting signal such as a rising edge.
The frequency I need is around 10 kHz at most.
Is there a component that would allow me to do this in a very precise way, with a built-in clock so as not to suffer from setting by external components? And to make sure that all the clock signals are perfectly synchronous?
Thank you so much !