This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00105: Can I connect multiple outputs in parallel to increase drive strength?

Part Number: LMK00105


I need to drive a 50 ohm cable with a clean clock source and I would like to parallel multiple outputs of the LMK00105 to drive a series 50 ohm resistor and then the cable.  Is this possible with this part?

  • Hi Andy,

    The output impedance of this buffer is 50 ohm. If you try to short them together then it would become 25 ohm. Unless your PCB trace is 25 ohm , you would want to add a series resistor of 25 ohm to match the impedance with transmission line which is usually 50 ohm. I think this would defeat the purpose of how you wanted to get more drive strength.

    Best,

    Asim