I noticed that the TLC2934 is not recommended for new designs. It is currently designed onto several boards. Is there a recommended replacement for this device? It is being used as an adjustable clock from 50MHz to 100MHz. The ideal replacement would be a part that operates up to 85C. The TLC2934 is only rated to 75C. Any recommendations on alternative devices would be appreciated.