Part Number: LMK04832
Hi,
We are using LMK04832 in our design.
We are using 100MHz TCXO in OSCin.
And the outputs are 13.1072MHz, 23.04 MHz and 32.768MHz. all outputs are CMOS.
The VCO frequency is set 2949.12.
But when we are loading the configuration, the output frequency is not coming proper.
All output frequency is coming more than that of what we set.
For 13.172, 14.54 is coming
For 23.04, 27.35 is coming
For 32.768, 39,37 is coming.
We have seen below observation,
The SCORE showing in TICSPRO for 2949.12 VCO is 0.1
We have tried other VCO frequency with score more than 0.5 and the desired output is not coming. (Not our actual desired output, just generated few outputs to verify from set VCO).
Please let us know what is the SCORE and PDF2 value in frequency planner solution?
Also please suggest if the score is less than 0.5, whether LMK is not able to generate the set output?
If so, is there any other option to generate our required frequencies?
Please suggest.
Best Regards,
Shafeeq