Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5C33216: LMK5C33216 SPI timing T6 spec can not meet

Part Number: LMK5C33216

Hi Team, 

When we were doing the LMK5C33126 signal test, we saw that the T6 parameter of the SPI could not meet the requirement. I understand that this is the minimum time for the"sdo read" to send the data after the 33126 receives the clock signal, but if the oscilloscope probe is placed on the host end to test the sdo read , because there is a pcb trace, the test result does not meet the requirements. If the probe is placed on the 33126 device end because the signal reflection is serious, the signal has a large step, and the timing is also inaccurate. The picture below is our 33126 I don’t know if my understanding is correct, please help me to read the analysis, thank you!

Thanks. 

B.R.

Lucas