Part Number: LMX2594
Hello,
My customer wants to use the LMX2594 with the following conditions.
- REFIN = 10MHz / PD = 20MHz
- RFoutAP = 6800MHz / RFoutBP = Value between 100MHz and 200MHz
After setting as below using TICS Pro v1.7.2.0, 106.25MHz output was confirmed in RFoutBP. However, the PLL was not locked.

They tried to test under the same conditions after updating TICS Pro to the latest version, but the settings did not work as shown below.

How do they set up LMX2594 to use it with the above settings? Could you please provide an example setup for the latest TICS Pro?
Thank you.
JH