HI
I'm using the LMX2820EVM in a feedback with 2 mixers configuration.
The RF output frequency from LMX is 4.3GHz and there is mixer with 4GHz LO to down convert 300MHz IF. (There is a low pass filter on the output of the mixer )
The 300MHz IF down convert again to 30MHz by LO 330MHz that generated from DAC
My question is if I must/can used in LTC6957-1 (buffer - squire wave LVPECL ) because the input of the PFDIN is very low frequency (30MHz) and the slow rate is long.
Thanks ,
Porat.