Part Number: LMK03318
Hey,
We would some help to understand how we can change the base adresse.
We have everything configured and its working as expected - we create a epr which we are using to program the pll.
According to the datasheet we would need to change Byte 11 in the eeprom.
(1b)Import EEProm file to GUI MAP
Then we modify the byte 11 from A0 to 8 => 0x40 should be the new i2c adresse
(2)Write GUI Map to SRAM
(3)Program EEPROM from SRAM
But it is still 0x50.
Many thanks
Best Christoph