This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820: Duty Cycle for PFDIn and OSC_IN

Expert 1585 points

Part Number: LMX2820

Hi

We are using the device with direct input of the feedback signal to PFDin pin. 

The reference is connected to OSC in. 

Both inputs are single ended 50ohm. 

Both signals arrive from saturated amplifiers which generate even and odd harmonics, which transform in time domain to square wave with 65% duty cycle. 

Is there an importance to the duty signal of both signals? - besides the comment about the OSC doubler spurs. 

Thanks