Part Number: LMK04832-SP
Other Parts Discussed in Thread: LMK04832,
Hi,
I have verifying a design that includes the LMK04832 device. I am trying to assert the RESET to the LMK04832, but it doesnot generate the reset event. The schematic snippets of the RESET signal path are shown below - it is voltage translated from 1.5V to 3.3V and the signal also has a 10 Kohm pulldown in addition to AC termination. The voltage measured from the output of the voltage translator at R214 was ~1.945V when asserted, and 0V when deasserted, but the digital input VIH requirement is 1.2V min, so I am confused on why the reset is functioning properly. Could some tips be provided? Also, are there pull-up resistors (or any sort of terminations) that are internal to the LMK04832-SP device on the RESET/GPO pin?


Thanks!