This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832EVM: 10MHz in and 100MHz out x 5

Part Number: LMK04832EVM
Other Parts Discussed in Thread: LMX2820, LMK04832, CDCE6214

Hello,

I need something to take a 10MHz clock input and generate 5 x 100MHz clocks that are all in phase.

I This evm capable of doing this or do I need something like an LMX2820 to do the 10 to 100MHz and then this for the distribution?

Thanks;

Leo