Part Number: CDCE421A
Other Parts Discussed in Thread: LMK61E2
I have not been able to get the CDCE421A to react to any command over SDATA.
I'm using a custom PIO programing on a RP2040 microcontroller to handle the the pulsing and timing which works well based on the result on seeing on the output.
The PIO code is as follows:
.program cdce421a
.side_set 1 opt
.define public T1 2
.define public T2 6
.define public T3 2
pull_data:
pull block
out y, 4
bitloop:
jmp !y pull_data side 0 [T3 - 2]; Side-set still takes place when instruction stalls
out x, 1
jmp !x do_zero side 1 [T1 - 1]; Branch on the bit we shifted out. Positive pulse
do_one:
jmp y-- bitloop side 1 [T2 - 1] ; Continue driving high, for a long pulse
do_zero:
jmp y-- bitloop side 0 [T2 - 1] ; Or drive low, for a short pulse
% c-sdk {
#include "hardware/clocks.h"
static inline void cdce421a_program_init(PIO pio, uint sm, uint offset, uint pin, float freq) {
pio_gpio_init(pio, pin);
pio_sm_set_consecutive_pindirs(pio, sm, pin, 1, true);
pio_sm_config c = cdce421a_program_get_default_config(offset);
sm_config_set_sideset_pins(&c, pin);
sm_config_set_out_shift(&c, false, false, 32);
//sm_config_set_fifo_join(&c, PIO_FIFO_JOIN_TX);
int cycles_per_bit = cdce421a_T1 + cdce421a_T2 + cdce421a_T3;
float div = clock_get_hz(clk_sys) / (freq * cycles_per_bit);
sm_config_set_clkdiv(&c, div);
pio_sm_init(pio, sm, offset, &c);
pio_sm_set_enabled(pio, sm, true);
}
It is initialized at 70 kHz, per the datasheet, in the main c file:
cdce421a_program_init(pio, sm, offset, CDCE421A_PIN, 70000);
Data is sent prepended with its size in bits to use as a counter in the PIO asm and shifted left out of the OSR.
static void cdce421a_write(uint32_t data, uint32_t bits) {
pio_sm_put_blocking(pio, sm, (data << (32 - bits - 4)) | (bits << 28));
}
I've defined the data accordingly:
#define ENTER_PROG_MODE cdce421a_write(0b001100,6) #define READBACK_MODE cdce421a_write(0b111011,6) #define WRITE_WORD_0 cdce421a_write(VCO_SEL_VCO1 | PRESCALER_DIV_BY_5 | OUTPUT_DIV_BY_8 | DRIVER_SEL_LVDS | TITEST1 ,11) #define WRITE_WORD_1_DEFAULT cdce421a_write(0x4FA,11) #define WRITE_WORD_2_DEFAULT cdce421a_write(0x2C0,11) #define WRITE_WORD_3_DEFAULT cdce421a_write(0x61E,11) #define WRITE_WORD_4_DEFAULT cdce421a_write(0x101,11) #define WRITE_WORD_5_DEFAULT cdce421a_write(0x500,11) #define EXIT_PROG_MODE cdce421a_write(0x7FF,11) #define PROG_EEPROM cdce421a_write(0x7F0,11) #define EXIT_PROG_EEPROM cdce421a_write(0x700,11)
This is what the readback mode waveform looks like:


I delay 1ms then send 0 pulses to read the EEPROM contents but the output oscillation never stops. I can tell because the clock drives a RISC-V core which I have running an LED binary counter application and it continues normally. If I disable the CDCE421A it halts the application. I'd expect the same behavior when in readback mode.
I've exhausted all options I can think of to get this working including reading the few posts about it here multiple times. Is there anything else I can try?