Part Number: CDCI6214
Other Parts Discussed in Thread: CDCE6214
Hi,
I wish to generate 2MHz clocks from channel 2 and 3. But the measured output clocks are always 760KHz. The input is 80MHz LVDS ac-coupled input.
Below figure is block diagram in TISC Pro. The input is bypassed to Y0. I can measure an 80MHz clock. So I don’t know why the outputs are 760KHz. The PLL is unlocked, but I tried several options, on one can lock it.
TICS Pro
80MHz output at Y0

760KHz output