Part Number: LMX2594
Other Parts Discussed in Thread: LMX2572
The problem with LMX2594 is that there are spurious emissions moving back and forth near the main signal.
The main signal is 4703.75M, clock ref 100M, Phase detection frequency 200M, moving spurious emissions disappear at 4700M. It seems to be related to the integer boundary
Another question:
Regarding the problem of LMX2594 integer boundary spurs. clock ref 100M, Phase detection frequency 200M, integer boundary spurs appear at integer multiples of 100M
Change the Phase detection frequency through the Multiplier Frequency divider and Frequency multiplier of the reference channel.
For example, if the phase detection frequency is changed to 233.33M or 160M or 240M, there will still be integer boundary spurs at integer multiples of 100M.
The integer boundary cannot be eliminated by changing the Phase detection frequency, but changing the reference frequency to 80M can eliminate spurious emissions at integer multiples of 100M, but integer boundary spurs appear at integer multiples of 80M.
My question is why changing the Phase detection frequency using Multiplier cannot eliminate integer boundary spurs, but changing the reference frequency can. Isn't the integer boundary defined by Phase detection frequency?
Also, the reference signal I used is a square wave. Does it have any impact?