Part Number: LM567C
Other Parts Discussed in Thread: LMC567
Hi Team,
Could anyone let me know why the recommended temp in the ds is -20 - 120C?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Noel,
Thanks. I just checked LMC567 and got a question about the pinout.
On the page 3 of the ds, pin 5 is marked as T-cap and pin 6 is marked as T-res, however in the typical application block diagram and the layout diagram on page 10 and page 12 they seem to be reversed(pin 5 is T-res and pin 6 is T-cap). Also I compared with LM567's pin setup and layout, and it seems like they got almost the same layout, while LM567 has it's pin 5 marked as T-res and pin 6 as T-cap.
Could you help check if the pinout on LMC567 ds is correct?
Also, I in 7.1 the device's maximum rating is 2Vp-p minimum for input voltage, could you elaborate what does this mean?(Is the minus mark missing here?)

Regards,
Hi David,
This part is pretty old, there are several errors in the datasheet, apologies.
2Vpp is the max. input voltage swing. VIH is Vcc + 0.5V.
Pin 5 should be T_res; Pin 6 is T_cap.