Part Number: LMK5B12204
Other Parts Discussed in Thread: LMK05318B
Hello team,
My customer is looking for a simple 1ch jitter cleaner with integrated clock divider.
The input frequency will change from 10MHz to 100MHz on the fly, and the output should be as low as 150kHz.
Questions:
- Can LMK5B12204 be used for this condition?
- Where should I input dirty clocks, XO input or Ref Input?
- Do I still need to input ref clock for DPLL, even if I don't need phase sync features?
Best Regards,
Kei Kuwahara