Part Number: LMX2694EPEVM
Other Parts Discussed in Thread: USB2ANY,
I am currently working on a development board for a PLL (lmx2694epevm) and I am not able to interact with via USB2ANY.
I have connected the 3.3V power (max 1A) to the board. Then I have connected a 100MHz reference clock at 0dbm, the programming cable and the RDOUTBM sma is connected to a high frequency oscilloscope.
However, USB2ANY is not able to identify the board after blinking.
I tested the power supply and it is 3.3V.
I measured some voltages on the board and it is
- 2.5V between VDD and GND and
- 3.3V between VDD and CE pin.
The oscilloscope at 40GHz is able to detect a different level of noise when it is powered up, however applying the FFT this is a low frequency noise.
Is there any way to understand if the board is functional or should I directly ask for a RMA?
Thanks in advance for any help.