Part Number: LMK04832
We're having trouble configuring the OSCout pins to a valid hardware configuration in the TICS PRO software.
We'll be using the OSCout as a buffered OSCin and we think we have this configured correctly in the CLKinX Control tab (Clock Format set to LVDS, OSCout_MUX is set to Buffered OSCin, and CLKin2_EN is set to 0). In the Clock Outputs tab we have OSCout set to LVDS, the mux is set to "Buffered OSCin" and the frequency for OSCout is the same as OSCin.
But, when we go to the Current Calculator tab it shows "Incorrect output termination" under the Hardware Configuration tab no matter what we set the termination to. The Current Calculator tab seems to be perfectly happy with the other 7 LVDS outputs set to Open, but nothing will give us a valid termination for the OSCout pin.