Part Number: LMK03318
HI Support,
1) Is "Export HEX register values" file generated by TICSpro the correct production programming file that should be used to program LMK03318 in production on virgin boards (using onboard I2C bus master for example processor)? Question is if LMK03318 will be FULLY programmed using this TICSpro output "Export HEX register values" file. LMK03318 is used in Soft Pin Mode - planning to use only one EEPROM page (one configuration).
2) It appears that "Export HEX register values" file generated by TICSpro has register addresses that aren't documented in datasheet. Do those need to be written and programmed into the device as well?
3) Datasheet indicates there are RESERVED bytes/registers and RESERVED bits within byte registers. Datasheet states: "Certain device registers and bits are reserved meaning that they must not be changed from their default reset state." Does this datasheet statement forces user to perform READ/MODIFY on RESERVED bytes/registers and registers with RESERVED bits within them?
4) Datasheet states: "Certain device registers and bits are reserved meaning that they must not be changed from their default reset state." Does this datasheet statement indicates that "Export HEX register values" file generated by TICSpro ISN'T everything needed in production to program the device because programming tool / software need to know the location of the reserved bytes and bits to perform READ/MODIFIY?
Best regards,
Adam