This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820: Which registers can be controlled to achieve output

Part Number: LMX2820


We set up a board with lmx2820, the software can not control the output at present. But register reads and writes are normal. For example, reset=1 and R0=0x4070. 

We did a few things on R32, 36, 42, 43, 38, 39, 78, 79,0, but RFOUTX_P just doesn't measure any signal.

Is there a quick output tutorial? Which registers must be set and what value should be set?

For starters, the 2820's manual is a little less friendly.

I look forward to your help. Thank you