We are using TI's clock generator (LMK series). However, we are reviewing CDCE6214-Q1 due to the following problems.
The first major problem is the frequency change time, and the second problem is that you only want to change the frequency of one channel,
but when you change the frequency, both channels stop for a moment.
CDCE6214-Q1 Device is
-. Is it possible to change the frequency within 1ms?
-. I'm using two channels, and I'm only going to change the frequency of one channel, and I want the other channel to come out without interruption.
change frequency time : about 2.6ms (LMK series)
yellow : out0
green : out1
blue : I2C