Part Number: LMX1204
I have a custom board design with an LMX1204 chip, if I look at the chip it has P as a postfix (LMX2594P), so I assume it is a preliminary version of LMX1204. I used the TicsPro Ver 1.7.2 which programmed the part successfully. I was not able to program the chip on the newer board and observed that the chip doesn't have the P as a postfix, so I assume it is production version. Now I am using the TicsPro Ver 1.7.5.15 to program the production version chip but for some reason, it never gives the output. The following are the questions:
1 - Am I using the correct version of TicsPro that I was supposed to use?
2 - Are there any other modifications between preliminary and production chips other than the register map?
3 - I have verified the input clock signal and power supplies for the LMX1204 chip they all are good. What else I should look for?
4 - Are there any known issues with the LMX1204P (Preliminary) oscillating?
Thanks,
Shehezad