Part Number: LMK05028EVM
Other Parts Discussed in Thread: LMK05028, LMK5C33216, LMK5B33216, LMK05318B, LMK5C33216A, LMK5C33216EVM
Hello
I bought a LMK05028 EVM. I have several questions
1) Do you know where I can find the initial .tcs file that is load into the EEPROM?
I would like to modify it and test with our generator that can give maximum 5 MHz instead of 25MHz ( EVM Quick Start, snau223).
2) With the LMK05028 EVM, I would connect a PPS to IN0 (1Hz) and I would like to have the following ouputs:
- A PPS (out 0) in LVDS,
- 38,4 MHz synchronised to the input PPS and phase aligned with PPS out0,
Do you have .tcs file for testing?
Thank you
best, regards
Patrice