This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE913 output clock behavior when updating frequency setting

Other Parts Discussed in Thread: CDCE913

We are considering using the CDCE913 for video clock generation. For our project we need to be able to adjust the frequency of the clock source smoothly, for example when changing from 80MHz to 81MHz we need the clock to smoothly transition to the new settings, with no output clock signal interruptions and with only small changes in duty cycle and period. In ideal case the clock period _n_ would be with old setting and clock period _n+1_ with the new setting. Is this possible with the CDCE913 if we would only change the frequency in small steps (few percent max) ?

Thank you for Your answer

Best regards

Filip Roth