Part Number: LMX2595
Hi
We want to use the LMX2595 to generate an 20GHz signal to feed to the LO ports on two mmWave IC's.
Is it possible to use port A for one mmWave IC's LO input and port B for the other IC, but still have the same phase and same propagation delay with matched PCB trace lengths?
What are the maximum expected delays?
Alternatively we need to split for example RFoutA into two signal traces.
Thank you in advance
Best Regards
Adrian