This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05318B: If want the output synchronized with PRIREF all the time, which mode should I chosen,free-run or holdover

Part Number: LMK05318B

Here is my config file now.

XO =24.000 MHz, REF=8KHz,CH7 = 24.576 MHz.tcs

This configuration currently encounters two issues:

  1. The PRIREF clock input is available after the operation of LMK05318B registers.
  2. The PRIREF clock input may be interrupted and restored later due to gPTP.

Although output7 generates a 24.576MHz signal, but it is observed on an oscilloscope that PRIREF and output7 are not phase synchronized.

Is there any method to automatically sync output7 with PRIREF without restarting LMK05318B? Currently, it is found that after restarting LMK05318B while PRIREF is functioning normally, the two frequencies can be synchronized.