This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592: PLL device that can use GPS(1PPM) as a reference clock

Guru 12645 points

Part Number: LMX2592
Other Parts Discussed in Thread: LMK05318B

Hello,

My customer is looking for a PLL device with the conditions below.

   - Ref Clock : TCXO 10MHz or GPS (1PPM)

   - Output clock : 6.3~6.9GHz

They prefer products that allow them to select TCXO 10MHz and GPS (1PPM) as reference clocks. However, if there is no such product, please introduce a product that can use GPS as a reference clock.

Thank you.

JH

  • Hi JH, 
    We don't have a single IC solution capable of this... 
    The only workaround would be to take a DPLL device such as LMK05318B which can take a 1PPS input *(or the 10 MHz TCXO input) and then have the output of that device drive an RF synthesizer to generate the HF outputs. 

    Regards, 

    Vicente