Part Number: LMX2594
Other Parts Discussed in Thread: TPS7A4501M
Hi,
Pl. advice about grounding scheme for LMX2594 if we are using two such LMX2594 in single card along with TCXO and TPS7A4501M to avoid coupling of outputs and interference.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2594
Other Parts Discussed in Thread: TPS7A4501M
Hi,
Pl. advice about grounding scheme for LMX2594 if we are using two such LMX2594 in single card along with TCXO and TPS7A4501M to avoid coupling of outputs and interference.
Hi, Apart from above mentioned query, LMX2594 Data sheet suggest (page number 65) if not used, RampClk, RampDir and SysRefReq can be grounded on the DAP.
Question : Grounding is required directly or using 1 KOhm register. ?
We are also not using Sync pin. so can we ground it with DAP?
Hi There,
The used pins can be short to ground directly or via a small resistor.
Datasheet Page 75 has the recommended land pattern.
The name of the GND pin tells which building block is using it, we need to connect these GND together externally. I don't see a real benefit to separate these GND.