Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595, LMK61PD0A2, LMX2485E
Hello Sir,
We plan to use two PLL to generate an 12.8GHz LO.
Use SYN1 to generate the 100 MHz , use the SNY2(LMX2595) (with the 100MHz reference)to generate a final 12.8GHz LO. There is an outside 10MHz or 50MHz for external reference.
We are trying to find the SYN1 which could provide an 100MHz reference to the LMX2595.
The goal is to get the 12.8GHz LO synchronize to the external 10MHz.
If we use the reference pro LMK61PD0A2 to generate the 100MHz reference, we are not sure how to synchronize the 10MHz reference?
Is that possible to use the Synchronize pin of the LMX2595?
Best Regards,
Kevin Zheng
RF Engineer