Part Number: LMX2572
Hi There,
question, without resorting to buying an eval board....
at an output frequency near 340 MHz,
(I am happy with whatever you have on file from 300 to 600 MHz)
being an INTEGER multiple of the reference frequency
(so that the chip is in integer mode and fractional spurs are not in play)
What are the levels of the spurs within +/- 50 MHz of the carrier ?
(these will be harmonics of the reference and other ?)
IE I need a spectrum plot .
(and the phase noise plots in the datasheet do not have any information on what mode the chip was in. )
Regards,
Robert