What is the output state or behavior when the inputs are floating or at least are not toggling? Are they held at certain levels, held at their previous levels, or something else?
Section 8.3.1 of the January 2022 datasheet talks about the "Fail-Safe Input" feature, which implies that if the inputs are floating the part won't oscillate, which I assume means the outputs will not toggle. If you could confirm that would be helpful, if it's possible to say the exact state of the outputs when inputs are floating/not toggling, that would be greatly appreciated.
Thanks,
Andy