This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: Frequency sweep time question

Part Number: LMX2595

hello.

We want to control the 12.17GHz to 12.235GHz range with LMX2595 in 0.5MHz Step. (Control mode or Ramping mode)
(ex: 1: 12.170GHz -> 2: 12.1705GHz, 3: 12.171GHz ... )

Can I know the time it takes to control with 0.5MHz Step?
(I wonder if the control time between steps is within 10us.)

The MCU used is FPGA (XC7K70T-1FBG484I).