Hi,
We use the SYNC feature in mode 2 (fout is integer multiple of foscin, input MULT/Doubler off) with FULL ASSIST.
Using internal feedback (not using PFDIN) it works fine.
Using external feedback, RFOUT becomes unstable/noisy as soon as R1:PHASE_SYNC_EN is set.
This happens even before the PSYNC pulse is actually applied.
When the PSYNC pulse is sent, RFOUT looks fine (searching for target phase?) for about 130 us.
After that, it becomes unstable/noisy again.
Are there general limitiations with using the SYNC feature in external feedback mode (offset loop) configuration?
Thanks & Best regards
David