Part Number: LMK04832
Hi
I have a question on LMK04832, Regarding clock group and clock frequency.
Is there a relationship between Clock group and Clock frequency?

- Is the clock group should have same frequency?
- For eg., CLKOUT6, CLKOUT8 should have same frequency?
- OR They can be different frequency?
- Are the clock group shall have same IO Standard?
- For eg., CLKOUT6, CLKOUT7 (DCLK's) should be of same IO Standard?
- Power supply side, I will be filtering each clock group through separate ferrite bead.
Also, I've attached the different clock scheme based on clock grouping
Can you please let me know which one would be best for my case?
BITE clock would be 3.2GHz (VCO Frequency without any divider)
Clock scheme on clock group has considered
1) pcb layout (3U card)
2) clock grouping so that noise will be minimised.
I would welcome your suggestions or feedback.